By pressing the
button located on the Toolbar on the Realtime OS Task Analyzer panel, the user can clear the analysis information that is displayed in the Child-panel display area.
![](r20ut2891ej0103_ri85v4rhan-29.gif)
![](r20ut2891ej0103_ri85v4rhan-30.gif)
By pressing the
button located on the Toolbar on the Realtime OS Task Analyzer panel, the user can clear the analysis information that is displayed in the Child-panel display area.