This section describes the API functions output by the Code Generator, using the following notation format.

Indicates the name of the API function.
Outlines the functions of the API function.
Indicates the format to be used when describing an API function to be called in C language.
API function arguments are explained in the following format.
API function return value is explained in the following format.