Changes the output voltage of D/A converter.(12bit mode)
[Syntax]
#include “r_cg_macrodriver.h”
void R_DACn_Change_OutputVoltage ( uint16_t outputVoltage );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
I |
uint16_t outputVoltage; |
output Voltage (Low 12bit) |
[Return value]
None.