Everything

r_pga_dsad_interrupt_conversion

Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.

Remark         This API function is called as the interrupt process corresponding to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_pga_dsad_interrupt_conversion ( void );

 

CC-RL Compiler

static void   __near r_pga_dsad_interrupt_conversion ( void );

 

[Argument(s)]

None.

 

[Return value]

None.