Everything

R_RTC_Set_ConstPeriodInterruptOn

Sets the cycle of the interrupts INTRTC, then starts the cyclic interrupt function.

 

[Syntax]

#include       “r_cg_macrodriver.h”

#include       “r_cg_rtc.h”

MD_STATUS   R_RTC_Set_ConstPeriodInterruptOn ( rtc_int_period_t period );

 

[Argument(s)]

I/O

Argument

Description

I

rtc_int_period_t period;

Interrupt INTRTC cycle

  HALFSEC:           0.5 seconds

  ONESEC:             1 second

  ONEMIN:              1 minute

  ONEHOUR:         1 hour

  ONEDAY:             1 day

  ONEMONTH:      1 month

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument specification