Performs processing in response to the frequency error interrupt.
Remark This API function is called to run interrupt processing for the frequency error interrupt, which is generated when the clock frequency is not in the allowed range (from the minimum to the maximum value).
[Syntax]
static void r_cac_ferrf_interrupt ( void );
[Argument(s)]
None.
[Return value]
None.