Performs processing in response to the voltage monitoring n interrupt.
Remark This API function is called to run interrupt processing for the voltage monitoring n interrupt, which is generated when the voltage detection circuit detects the voltage being dropped.
[Syntax]
static void r_lvd_lvdn_interrupt ( void );
Remark n is the circuit number.
[Argument(s)]
None.
[Return value]
None.