Everything

r_riicn_error_interrupt

Performs processing in response to the transfer error/event generation interrupts (EEI).

Remark         This API function is called to run interrupt processing for the transfer error/event generation interrupts (EEI), which are generated when the I2C bus interface detects the transfer error/event generation (arbi-tration-lost, NACK, timeout, start condition, and stop condition).

 

[Syntax]

static void    r_riicn_error_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.