Everything

R_RTC_Set_BinaryAlarm

Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode).

 

[Syntax]

void    R_RTC_Set_BinaryAlarm ( uint32_t alarm_enable, uint32_t alarm_val );

 

[Argument(s)]

I/O

Argument

Description

I

uint32_t alarm_enable;

Comparison flag

0x0                                             : Comparison does not proceed

0x1                                             : Comparison proceeds

I

uint32_t alarm_val;

The value of the binary counter

 

[Return value]

None.