Performs processing in response to the transmit-end interrupts.
Remark This API function is called as the r_scifan_teif_interrupt callback routine.
[Syntax]
static void r_scifan_callback_transmitend ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.