Starts SCI master transmission/reception (simple SPI mode).
Remark 1. This API function repeats SCI master transmission in byte units the number of times specified by the argument tx_num from the buffer at the location specified by the argument tx_buf.
Remark 2. This API function repeats SCI master reception in byte units the number of times specified by the argument rx_num and the received data are stored in the buffer at the location specified by the argument rx_buf.
Remark 3. When performing a SCI master transmission/reception, R_SCIn_Start must be called before this API function is called.
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_SCIn_SPI_Master_Send_Receive ( uint8_t * const tx_buf, uint16_t tx_num,
uint8_t * const rx_buf, uint16_t rx_num );
Remark n is the channel number.
[Argument(s)]
| I/O | Argument | Description | 
| I | uint8_t * const tx_buf; | Pointer to a buffer storing the transmission data | 
| I | uint16_t tx_num; | Total amount of data to send | 
| O | uint8_t * const rx_buf; | Pointer to a buffer to store the reception data | 
| I | uint16_t rx_num; | Total amount of data to receive | 
[Return value]
| Macro | Description | 
| MD_OK | Normal completion | 
| MD_ARGERROR | Invalid argument tx_num specification |