Everything

R_TPU_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer pulse unit.

Remark         This API function is called as the R_TPU_Create callback routine.

 

[Syntax]

void    R_TPU_Create_UserInit ( void );

 

[Argument(s)]

None.

 

[Return value]

None.