Confirm the source code (device driver program) that reflects the information configured as described in "2.3 Enter Information".
To confirm the source code, use the Code Preview panel that opens by double-clicking [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview] >> Peripheral function node >> Source code node (>> API function node) in the Project Tree panel.

You can change the source code to be displayed by selecting the source file name or API function name in the Project Tree panel. |
The following table displays the meaning of the color of the source code text displayed in the Code Preview panel. |
You cannot edit the source code within the Code Preview panel. |
For some of the API functions, values such as the register value are calculated and finalized when the source code is generated (when the |