20.8	 Domain Definition (domain[])
 Here, each domain is defined. The domain that is not defined by this static API is handled as "trust = NO".
 
 Parentheses < >show the user input part. 
 
 -	 Description
Define the domain ID number.
 
 -	 Definition format
Numeric value
 
 -	 Definition range
From 1 to 15
 
 -	 When omitting
Cannot be omitted.
 
 2 )	 Trusted domain (
trust)
 
 -	 Definition format
Symbol
 
 -	 Definition range
Select either of the following:
 
 YES:	The domain is trusted domain.
 
 OFF:	The domain is not trusted domain.
 
 -	 When omitting
The set value in the default system configuration file (factory setting: "NO") applied.