act_tsk
iact_tsk
ER act_tsk (ID tskid);
ER iact_tsk (ID tskid);
 These service calls move the task specified by parameter tskid from the DORMANT state to the READY state.
 As a result, the target task is queued at the end on the ready queue corresponding to the initial priority and becomes subject to scheduling by the RI600V4.
 If the target task has been moved to a state other than the DORMANT state when this service call is issued, this service call does not move the state but increments the activation request counter (by added 1 to the activation request counter).
 Note 1	 The activation request counter managed by the RI600V4 is configured in 8-bit widths. If the number of activation requests exceeds the maximum count value 255 as a result of issuing this service call, the counter manipulation processing is therefore not performed but "E_QOVR" is returned.
 Note 2	 Extended information specified in Task Information (task[]) is passed to the task activated by issuing these service calls.