tloc_mtx
ER tloc_mtx (ID mtxid, TMO tmout);
 If the target mutex could not be locked (another task has been locked) when this service call is issued, this service call queues the invoking task to the target mutex wait queue and moves it from the RUNNING state to the WAITING state with time-out (mutex wait state).
 When the mutex is locked, this service call changes the current priority of the invoking task to the ceiling priority of the target mutex. However, this service call does not change the current priority when the invoking task has locked other mutexes and the ceiling priority of the target mutex is lower than or equal to the ceiling priority of the locked mutexes.
 Note 1	 Invoking tasks are queued to the target mutex wait queue in the priority order. Among tasks with the same priority, they are queued in FIFO order. 
 Note 2	 This service call returns "E_ILUSE" if this service call is re-issued for the mutex that has been locked by the invoking task (multiple-locking of mutex).
 Note 3	 TMO_FEVR is specified for wait time tmout, processing equivalent to loc_mtx will be executed. When TMO_POL is specified, processing equivalent to ploc_mtx will be executed.