13.3 System Information
 The following describes the format that must be observed when describing the system information in the system configuration file.
 The GOTHIC-FONT characters in following descriptions are the reserved words, and italic face characters are the portion that the user must write the relevant numeric value.
 Specifies the system stack size (in bytes).
A value between 0 and 65534, aligned to a 2-byte boundary, can be specified for sys_stksz.
A value between 0 and 65534, aligned to a 2-byte boundary, can be specified for sys_stksz.
 Note 2	 For details about the estimation of the system stack size, refer to See "13.5.1System stack size".