Everything
3.1.2 Assemble list

The location counter value, code, line number, and source program under assembly is output.

The output example of the assemble list is shown below.

(1)       (2)                 (3) (4)
OFFSET    CODE                NO  SOURCE STATEMENT
 
00000000                       1  #CC-RH Compiler RH850 Assembler Source
00000000                       2  #@      CC-RH Version : VX.XX.XXx [DD Mmm YYY]
00000000                       3  #@      Command : main.c -Xcommon=rh850 -S
00000000                       4  #@      compiled at Sun Jan 1 00:00:00 2012
00000000                       5          .cseg text
00000000                       6          ld.w $_data,r12
00000000  440E0000              -- movhi       0x0,gp,r1
00000004  21670100              -- ld.w        0x0[r1],r12
00000008                       7
00000000                       8          .dseg data
00000000  00000000             9  _data:  .dw 0
00000004                      10

Number

Description

(1)

Location counter value

The location counter value for the beginning of the code generated for the source program of the corresponding line is output.

(2)

Code

The code (machine language instruction or data) generated for the source program of the corresponding line is output.

Each byte is expressed as 2-digit hexadecimal number.

(3)

Line number

The number of the line is output.

This is expressed in a decimal number.

(4)

Source program

The source program of the line is output.

If instruction expansion is performed for the instruction at that line, the disassembly of the array of machine language instructions generated after the instruction expansion is displayed after "--".

Compiler information (lines 1 to 4) is output only when an assembly source file output from the compiler is assembled.