Everything
4.2.5 #pragma directive

Below are #pragma directives supported as extended language specifications. These extended specifications can also be used with the _Pragma operator in C99.

Table 4.10

List of Supported #pragma Directive