Everything
5.1.8 2-byte separation operators

The following 2-byte separation operators are available.

Operator

Overview

HIGHW

Returns the high-order 16-bit value of a term.

LOWW

Returns the low-order 16-bit value of a term.

HIGHW1

The value calculated by adding the value at the 15th bit to the uppermost 16 bits of the term.