Everything
5.3.3 File input control instructions

Using the file input control instruction, the assembler can input an assembler source file or binary file to a specified position.

The following file input control instructions are available.

Table 5.17

File Input Control Instructions

Control Instruction

Overview

INCLUDE

Quotes a series of statements from another source module file

BINCLUDE

Inputs a binary file