Everything
5.6 Predefined Macro Names

The assembler defines the following macros.

Predefined Macro Names

Remark

__RENESAS__

This value is set to 1.

__ASRH__

This value is set to 1.

__ASRH

This value is set to 1.

__RH850__

This value is set to 1.

__RH850

This value is set to 1.

__PIC

This value is set to 1. It is defined when the -pic option is specified.

__PIROD

This value is set to 1. It is defined when the -pirod option is specified.

__PID

This value is set to 1. It is defined when the -pid option is specified.