|
-change_message [V1.06 or later]
|
This option changes the message levels.
[Specification format]
-change_message=error[={num|num1-num2}[, ...]]
|
- | Interpretation when omitted |
Message levels are not changed.
[Detailed description]
- | This option changes the specified warning messages to error messages.
This option controls message numbers W0510000 to W0549999. |
- | The rightmost 5 digits of the message number are specified for num, num1, and num2.
If a message number that does not exist is specified, it will be ignored. |
- | If no message number is included, operation is as if all message numbers have been specified. |
- | If num1-num2 is specified, it is assumed that message numbers within the range have been specified. |
- | If this option is specified more than once, all of the given specifications will be effective. |