This option specifies the maximum byte count for a data record.
[Specification format]
 
-  | Interpretation when omitted  | 
 
When the -form=hexadecimal option is specified, an Intel HEX file is generated assuming that the maximum byte count is "0xFF".
When the -form=stype option is specified, a Motorola S-record file is generated assuming that the maximum byte count is "0x10".
[Detailed description]
-  | This option is used to specify the length of data records in Intel HEX files or Motorola S-record files to be generated.  | 
 
-  | Values from 01 to FF (hexadecimal) are specifiable for Intel HEX files.  | 
 
-  | The following ranges of values are specifiable for Motorola S-record files.  | 
 
-  | S1 records: 01 to FC (hexadecimal)  | 
 
-  | S2 records: 01 to FB (hexadecimal)  | 
 
-  | S3 records: 01 to FA (hexadecimal)  | 
 
[Example of use]
-  | To specify 0x10 as the maximum byte count for a data record, describe as:  | 
 
>rlink a.obj b.obj -form=hexadecimal -byte_count=10 
 | 
 
[Remark]
-  | When the -form={hexadecimal|stype} option is not specified, this option will be invalid.  |