This option outputs the S9 record at the end.
[Specification format]
 
-  | Interpretation when omitted  | 
 
None
[Detailed description]
-  | This option outputs the S9 record at the end even if the entry point address exceeds 0x10000.  | 
 
[Example of use]
-  | To output the S9 record at the end, describe as:  | 
 
>rlink a.obj b.obj -form=stype -output=c.mot -s9 
 | 
 
[Remark]
-  | If the -form=stype option is not specified, this option will be invalid.  |