Everything

>=


Compares whether value of first term is greater than or equivalent to the value of the second term.

[Function]

Returns 1 (True) if the value of the 1st term of an expression is greater than or equal to the value of its 2nd term, and 0 (False) if the value of the 1st term is less than the value of the 2nd term.