Everything
5.3.2 File input control instructions

Using the file input control instruction, the CC-RL can input an assembly source file or binary file to a specified position.

The following file input control instructions are available.

Table 5.26

File Input Control Instructions

Control Instruction

Overview

INCLUDE

Inputs an assembly language source file

BINCLUDE

Inputs a binary file