CC-RX is a program that converts programs written in C/C++ or assembly language to a machine language.
CC-RX is comprised of the four executable files listed below.
(3) rlink: Optimizing linkage editor
Figure 1.1 illustrates the CC-RX processing flow.