| 
 Indicates the type for holding the necessary state of conversion between sequences of multibyte characters and wide characters.  | 
||
| 
 Equivalent to fwprintf with the variable argument list replaced by va_list.  | 
||
| 
 Converts the output format and writes data to an array of wide characters.  | 
||
| 
 Equivalent to swprintf with the variable argument list replaced by va_list.  | 
||
| 
 Equivalent to fwprintf with stdout added as an argument before the specified arguments.  | 
||
| 
 Equivalent to wprintf with the variable argument list replaced by va_list.  | 
||
| 
 Inputs and converts data from the stream under control of the wide string and assigns it to an object.  | 
||
| 
 vfwscanf <-lang=c99>  | 
 Equivalent to fwscanf with the variable argument list replaced by va_list.  | 
|
| 
 Converts data under control of the wide string and assigns it to an object.  | 
||
| 
 vswscanf <-lang=c99>  | 
 Equivalent to swscanf with the variable argument list replaced by va_list.  | 
|
| 
 Equivalent to fwscanf with stdin added as an argument before the specified arguments.  | 
||
| 
 vwscanf <-lang=c99>  | 
 Equivalent to wscanf with the variable argument list replaced by va_list.  | 
|
| 
 Inputs a wide character as the wchar_t type and converts it to the wint_t type.  | 
||
| 
 Equivalent to putwc with stdout specified as the second argument.  | 
||
| 
 These convert the initial part of a wide string to double, float, or long double representation.  | 
||
| 
 These convert the initial part of a wide string to long int, long long int, unsigned long int, or unsigned long long int representation.  | 
||
| 
 Copies a wide string and appends it to the end of another wide string.  | 
||
| 
 Copies a wide string with n or fewer wide characters and appends it to the end of another wide character string.  | 
||
| 
 Searches for a specified wide string in another wide string.  | 
||
| 
 Checks if a wide string contains another specified wide string.  | 
||
| 
 Searches for the first occurrence of a specified wide string in another wide string.  | 
||
| 
 Searches for the last occurrence of a specified wide character in a wide string.  | 
||
| 
 Calculates the length of the maximum initial segment of a wide string, which consists of specified wide characters.  | 
||
| 
 Searches for the first occurrence of a specified sequence of wide characters in a wide string.  | 
||
| 
 Divides a wide string into a sequence of tokens delimited by a specified wide character.  | 
||
| 
 Searches for the first occurrence of a specified wide character within the first n wide characters in an object.  | 
||
| 
 Checks if a specified object indicates the initial conversion state.  | 
||