Execute a service call process.
Figure A-32. ServiceCall Dialog Box
The following items are explained here.
[Description of each area]
(1) Service call display area
This area displays the service call selected in the context menu, in C format.
Remark If the service call requires a value to be input, a text box will appear in this area. Enter the value in question, then click [OK] to run the service call process.
|
|
|
Execute a service call process.
|
|
Ignore the setting and closes this dialog box.
The function of this item is same as that of the ![](images/ridb_D_ServiceCall2.jpg)
button.
|