| 
 Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20]  | 
This dialog box is used to display and change the detailed information on the timer event selected on the Events panel. Note that you cannot edit the address value of the timer event in this dialog box. If you need to edit the address value, first delete the timer event and then create a new one. For details on timer event setting, see "2.15 Measure Execution Time of Programs".
This section describes the following.
On the Events panel, move the caret to the timer event of which you wish to change the detailed information, then select [Edit Condition ...] from the context menu.  | 
In this area, detailed information on the timer event selected in the Events panel is displayed by category in the list. Also, you can directly change its settings.
In this area, brief description of the categories and properties selected in the detailed information display/change area is displayed.
| 
 Displays categories in the detailed information display/change area.  | 
|
| 
 Hides categories in the detailed information display/change area and rearranges only property items in the ascending order.  | 
[Description of each category]
You can display and modify the detailed settings on timer measurement.