2.14.6.1  
Change display mode
 
Display mode can be changed to the purpose when clicking the buttons below in the toolbar. 
Note that these buttons are disabled while the tracer is running. 
Table 2.15  | Display Modes of Trace Panel  | 
 
| 
 | 
 | 
 | 
| 
 
 
  
 | 
 
Mixed display mode 
 | 
 
Displays the instruction (disassemble results), labels, source text (corresponding source line), point trace results, and break causes (default).   
 | 
| 
 
 
  
 | 
 
Disassemble display mode 
 | 
 
Displays the instruction (disassemble results), labels, point trace results, and break causes.  
 | 
| 
 
 
  
 | 
 
Source display mode 
 | 
 
Displays the source text (corresponding source line), and break causes. 
However, when a place where no debugging information is present is executed, "<No Debug Information>" is displayed.  
 | 
 
Figure 2.72  | Example of Source Display Mode View (Trace Panel)  |