To clear the collected trace data contents, click the 
 button on the toolbar. 
Note that this button is disabled while a tracer is running.
When [Yes] is selected in the [Clear trace memory before running] property in the [Trace] category on the [Debug Tool Settings] tab of the Property panel, the trace memory is cleared each time a program is executed.  |