To set a Timer Result event, set a timer start event and a timer end event that starts/stops a timer measurement.
Use one of the following methods to set a timer start event and a timer end event.
The execution time of a desired section can be measured by setting execution-related events as timer start and end events.
Perform this operation in the Editor panel/Disassemble panel in which the source text/disassembled text is displayed.
Follow the operation listed below from the context menu, in accordance with your desired event type, after moving the caret to the target line that has a valid address.
| Select [Timer Settings] >> [Start Timer] >> [Set Timer nNote] | |
| Select [Timer Settings] >> [Stop Timer] >> [Set Timer nNote] | 
| [Simulator] | 
| The time for a timer end event will not included in the measurement results. For this reason, set a timer end event to one line below the range for which you wish to measure the run time. | 
A timer start event or a timer end event is set to the instruction at the start address corresponding to the line of the caret position.
Once a timer start event or a timer end event is set, the following event mark is displayed in the event area of the line/address that an event is set.
 
In this product version, this function is not supported.
When a timer start event and a timer end event are set, they are managed collectively on the Events panel as one instance of a Timer Result event (see "2.19 Manage Events"). When you click the "+" mark at a Timer Result event item, detailed information on the timer start event and the timer end event you have set is displayed.
 
| Example of Timer Start and Timer End Events (Execution Type) in Events Panel [Full-spec emulator][E1][E20] | 
 
| Event marks differ depending on the event state (see "2.19.1  Change the state of set events (valid/invalid)").  | 
| [Full-spec emulator][E1][E20] | 
 
  
  ) is displayed meaning more than one event is set at the point.
) is displayed meaning more than one event is set at the point.