The display format of the [value] area can be changed using buttons below on the toolbar.
|
The following buttons to change the notation of a data value are displayed. |
||
|
Displays the value of the selected watch-expression in the default notation (see "Table A.7 Display Format of Watch-Expressions (Default)") according the type of variable (default). |
||
|
Displays the value of the selected item in hexadecimal number. |
||
|
Displays the value of the selected item in signed decimal number. |
||
|
Displays the value of the selected item in unsigned decimal number. |
||
|
Displays the value of the selected item in float. Note that this item becomes valid only when the selected watch-expression value is 4-byte data. |
||
|
Displays the value of the selected item in double. Note that this item becomes valid only when the selected watch-expression value is 8-byte data. |
||
|
Adds the value in hexadecimal number enclosing with "()" at the end of the value of the selected item (except the item displayed in hexadecimal number). |
||
AutoSelect
Hexadecimal
Signed Decimal
Unsigned Decimal
Octal
Binary
ASCII
Float
Double