CS+ is a platform of an integrated developing environment for RH850 family, RX family, V850 family, RL78 family, 78K0R microcontrollers, 78K0 microcontrollers.
CS+ can run all the operations needed for developing the programs such as designing, cording, building, debugging, and flash programming.
In this manual, the debugging is explained out of those operations needed for the program development.
When the E2 emulator Lite (abbreviated name: E2 Lite) is used, please read references to "E1" in this manual as also meaning "E2 Lite". |
In this chapter, an overview of debugging products that CS+ provides is explained.