Everything
2.12.6.2 Change display format of values

The display format of the [Line Number/Address], [Address] [IECUBE][Simulator] and [Data] [IECUBE][Simulator] area can be changed using buttons below on the toolbar.

Note that these buttons are disabled while the tracer is running.

Notation

The following buttons to change the notation of a data value are displayed.

 

Hexadecimal

Displays values on this panel in hexadecimal number (default).

Decimal

Displays values on this panel in decimal number.

Octal

Displays values on this panel in octal number.

Binary

Displays values on this panel in binary number.