Everything
2.12.7 Clear the trace memory

To clear the collected trace data contents, click the button on the toolbar.

Note that this button is disabled while a tracer is running.

Remark 1.

[IECUBE][Simulator]
When [Yes] is specified in the [Clear trace memory before running] property in the [Trace] category on the [Debug Tool Settings] tab of the Property panel, the trace memory is cleared each time a program is executed.

Remark 2.

[E1][E20][EZ Emulator][COM Port]
The trace memory is cleared each time a program is executed (fixed).