The contents of the CPU register (general-purpose register/control register) can be shown and the value can be changed in the CPU Register panel below.
Select the [View] menu >> [CPU Register].
For details on the contents and function in each area, see the section for the CPU Register panel.
![](Debug_RL78_E-180.gif)
This section describes the following.
2.10.2.1 Change display format of values
2.10.2.2 Modify the CPU register contents
2.10.2.3 Display/modify the CPU register contents during program execution