Everything
2.10.3.2 Organize SFRs

The each SFR can be categorized (by folders) and displayed in the tree view.

Caution 1.

Categories cannot be created within categories.

Caution 2.

SFRs cannot be added or deleted.

(1)

Create new category

Move the caret to the SFR name to create a new category then click the button in the toolbar and directly enter the new category name.

(2)

Edit category name

Click the category name to edit, and click it again, then directly modify the category name from the keyboard.

(3)

Delete categories

Select categories to delete then click the button in the toolbar.

However, the categories that can be deleted are only the empty categories.

(4)

Change the display order

SFR name is categorized when SFR is dragged and dropped in the category.

Also, the display order of the categories and the SFR names (upper or lower position) can be changed easily by drag and drop operation.

(5)

Restore the category to its initial state

Click the button in the toolbar. The edited category is cleared and displayed with the initial category classification.