2.9.3
Stop the program at the arbitrary position (
breakpoint)
The program in execution can be stopped at the arbitrary position by setting a breakpoint. A breakpoint can be set by one-clicking with the mouse.
You need to configure the type of breakpoints to use before setting a breakpoint.
This section describes the following operations.
2.9.3.1 Set a breakpoint
2.9.3.2 Edit a breakpoint
2.9.3.3 Delete a breakpoint