This section describes how to execute programs.
The major operations discussed in this section can be conducted either from the debug toolbar or the [Debug] menu in the Main window, where commands to control the execution of programs are included.
Items in the debug toolbar and the [Debug] menu will be disabled once the connection with the debug tool is lost. |
![](Debug_RX_E-108.gif)
![](Debug_RX_E-109.gif)