This dialog box is used to move the caret to a specified line number, symbol, or address.
![](Editor_E-141.gif)
This section describes the following.
Focus the Editor panel, and then select [Go to...] from the [Edit] menu. |
On the Editor panel, select [Go to...] from the context menu. |
Directly enter the line number (decimal number), symbol nameNote 1 or addressNote 2 to which you want to move the caret.
"(valid line range)" shows the range of valid lines in the current file.
By default, the number of the line where the caret is currently located in the Editor panel is displayed.
On the Property panel of the build tool to be used, specify [Yes(-Xcref)][CC-RH][CC-RX]/[Yes(-cref)][CC-RL] with the [Output cross reference information] property, and then run and complete a build. |
Enter a hexadecimal number with prefix "0x" or "0X" added (a decimal number is handled as a line number). |