While a source file is open in the Editor panel, you can make CS+ recognize the currently selected string or the word at the position of the caret as a function or variable name and jump to the corresponding function or variable.
After a jump, the name of the given function or variable is indicated as being selected. If the compiler has not output cross-reference information, however, the jump to a function will be to the first line of executable code within the function, and jumping to variables will not work.
Select [Jump to Function or Variable] from the context menu after moving the caret to the target function or variable on the source text.
When multiple statements are described in a line, a jump to an illegal location may be made. |
For C++ source files [CC-RX] |
When a given character string does not fully specify the desired function, jumping may not be possible or the jump may actually be to a different function with the same name. |
Member functions in classes |
Functions defined in namespaces |
Template functions |
A jump to a variable is only possible when the compiler has output cross-reference information. |

Note that this function is available only when the following conditions are satisfied for each specific build tool.
When [Yes(-Xcref)][CC-RH][CC-RX]/[Yes(-cref)][CC-RL] is specified with the [Output cross reference information] property of the build tool |
If functions with the same name exist, then the Jump to Function dialog box will be opened, and you can select the jump destination function. |
When a function and a variable with the same name exist, the jump to the function takes precedence. |
When [No] is specified with the [Output cross reference information] property of the build tool, the scope of the operation becomes only functions, not variables |
The target function is defined in a file that is specified as the first file in the [Download files] property in the [Download] category on the [Download File Settings] tab of the Property panel. In addition, the file includes the symbol information. |
Calling the target function from the file corresponding to the address of the program counter (PC). |
When an external build tool is used, the scope of the operation becomes only functions, not variables |
The target function resides in an active project. In case it is disconnected from the debug tool, a jump to a static function cannot be made. |
A file with the symbol informationNote is specified with the [Download files] property in the [Download] category on the [Download File Settings] tab of the Property panel. In case it is disconnected from the debug tool, the above file is specified as the first file in the [Download files] property. |