This chapter describes the message types displayed by CS+.
 
The message types (1 alphabetic character) when CS+ is operated are as follows.
|  |  | 
|  | 
Internal error | 
Processing terminated (suspended) due to internal error. | 
|  | 
Fatal error | 
Processing terminated (suspended) due to fatal error. | 
|  | 
Information | 
Informational message.  Check the message and continue the process. | 
|  | 
Choice | 
This type of message is displayed when a choice is necessary in order to carry on with the next operation.  It performs the selected action. | 
|  | 
Warning | 
Warning message.  Check the message and continue the process. |