This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+.
The messages are classified by the message origination tool and displayed on the individual tabs.
| The Message area can be zoomed in and out by  | 
 
The following items are explained here.
The output messages of each tool are displayed.
Note that the character colors/background colors of the message differ with the type of output message (and depend on the settings in the [General - Font and Color] category in the Option dialog box).
Select the tab that indicates the origin of message.
The following tabs are available for the Pin Configurator.
| Displays operation logs for all components (design tool, build tool, etc.) provided by CS+ in order of output. | 
| Even if a new message is output on a deselected tab, tab selection will not automatically switch. In this case, " * " mark will be added in front of the tab name, indicating that a new message has been output. | 
| Sends the character string or lines selected with range selection to the clipboard. | |
| Selects all the messages displayed on the Message area. | |
| Deletes all the messages displayed on the Message area. | |
| Jumps to the caret line in the editor indicated by the message (file, line, and column). | |
| Displays help for the message on the current caret location. | 
 in the tool bar, or by operating the mouse wheel while holding down the [Ctrl] key.
 in the tool bar, or by operating the mouse wheel while holding down the [Ctrl] key.