This tab displays information about the pins connected to external peripherals in order grouped at the external-peripheral component level.
The following items are explained here.
On the Project Tree panel, double-click [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List]. |
On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List], and then press the [Enter] key. |
This area displays the “device pin list” for entering information on the pins connected to external peripheral parts.
Note that items in this area's device pin list are sorted by groups at the external peripheral controller level.
The following are the columns comprising the device pin list.
The following are the columns comprising the device pin list.
You cannot add information in the “External Peripheral Name”, “Connected Pins”, “Pin Number”, “Pin Name”, “Description”, “Recommend Connection for Unused” and “Attention” columns because they contain fixed information. |
If the “Free” in the “Function” column is changed to a specific pin name, color of the corresponding pin in the Device Top View panel changes from the “color representing the unused pins” to the “color representing the used pins” selected by clicking [Device Top View Settings] tab >> [Color] in the Property panel. |
To move columns (change the display order) in the device pin list, drag and drop the desired column to the desired location. |
To add the “user's own column”, use the New Column dialog box which opens by pressing the [New Column...] button in the Column Chooser dialog box which opens by pressing the |
button in the upper left corner of the device pin list.