|
csplus.download_loadmodule
|
This function downloads a file.
[Specification format]
csplus.download_loadmodule(session_id, file_path="", offset=0, load_image=True, load_symbols=True, clear_old_symbols=False, core_name="")
|
[Argument(s)]
|
|
|
|
session_id
|
This argument is ignored in this version.
|
|
file_path
|
Full path of the file to download.
|
|
offset
|
The offset to download the file at.
|
|
load_image
|
Specify whether to download image from the specified file.
|
|
load_symbols
|
Specify whether to download symbols from the specified file.
|
|
clear_old_symbols
|
Specify whether to add symbols from the specified file to current symbol table or overwrite symbol table in debugger.
|
|
core_name
|
The name of the core to download to.
|
[Return value]
None
[Detailed description]
- | If file_path is not specified or empty, download all loadmodules defined in launch configuration of the specified debug session, ignoring all other parameter's value. |
- | No reset happens after downloading, "csplus.reset_debug_session()" command need to be called manually. |
[Example of use]
>>> import sys
>>> sys.path.append("C:\Program Files (x86)\Renesas Electronics\CS+\CC\Plugins\PythonConsole\integration_service")
>>> import csplus
>>> csplus.connect()
>>> session_id = csplus.launch_debug_session("", True)
>>> csplus.download_loadmodule(session_id)
>>>
|