This is the start-up window that opens when CS+ is launched.
In this window, you can control the user program execution and open panels.
The following items are explained here.
- Select Windows [Start] >> [Programs] >> [Renesas Electronics CS+] >> [CS+].
[Description of each area]
This displays menus about real-time OS package.
|
|
Displays a cascading menu for relating to real-time OS package.
|
|
|
|
Opens the Realtime OS Resource Information panel.
|
|
|
Program analyzer is started.
Opens the AZ850V4 window.
Opens the AZ78K0R window.
|
|
|
Opens the Realtime OS Task Analyzer 1 panel.
[RI78V4 V2 .xx.xx][RI850V4 V2 .xx.xx][RI600V4]
|
|
|
Opens the Realtime OS Task Analyzer 2 panel.
[RI78V4 V2 .xx.xx][RI850V4 V2 .xx.xx][RI600V4]
|
The toolbar shows command buttons relating to real-time OS package.
|
|
Opens the Realtime OS Resource Information panel.
|
|
|
Opens the Realtime OS Task Analyzer 1 panel. [RI78V4 V2 .xx.xx]
[RI850V4 V2 .xx.xx][RI600V4]
|
|
|
Opens the Realtime OS Task Analyzer 2 panel. [RI78V4 V2 .xx.xx]
[RI850V4 V2 .xx.xx][RI600V4]
|
Panels are displayed in this area.