Everything

Appendix Contents of Information List Panel

Below chart describes contents of Function List Panel. For the details, refer to help.

"Static" information is described after build. "Dynamic" information is described after connecting the debug tool.

 

Description

Overview

Static/Dynamic

Function name

Function name defined/referenced in C source

Static

File name

File name of C source where the function is defined

Static

File Path

Absolute path of the C source file where the function is defined.

Static

Import

Source of the function information

Static

Attribute

Function's symbol attributes/symbol-modifier attributes

Static

Return Type

Return type of the function

Static

Arguments count

Argument value of the function

Static

Arguments

Argument type/formal argument name of the function

Static

Code Size

Function's code size

Static

Stack Size

Function's stack size

Static

Start Address

Function's start address

Static

End Address

End address of the function

Static

Reference Count

Number of times the function is referenced in the program

Static

Execution Count

Number of times the function was executed

Dynamic

Execution Time

Execution time of the function, Proportion of total, etc..

Dynamic

Code Coverage

Code coverage ratio of the function

Dynamic

Total

Total of above item in the target file

-